Quantità aggiornata
La quantità dell'ordine è stata aggiornata al minimo quantitativo vendibile
La quantità dell' ordine è stata aggiornata aCiò è dovuto alla confezione e alle quantità minime dell'ordine.
At Hilti we offer onsite testing to determine the strength of the materials supporting anchors and modular support systems.
Sometimes you can’t know about the resistance of key materials onsite, particularly if you’re working with existing concrete, natural stone, refractory stone, porous materials or wood.
And there may be no information available on the maximum load that they can carry and the maximum load, which can be assigned to an anchor.
So at Hilti we can carry out tensile tests to find the strength of the key base materials.
Our Hilti engineers are highly qualified and we regularly calibrate our testing equipment.
We work closely together with our customers onsite and test anchors according to the load that’s needed for the installation.
We provide a test report when we’ve finished, with test data and result.
Our onsite testing helps to:
QUICK LINKS
Per visualizzare i prezzi specifici, scegli il tuo account.